2024-11-18 5:45 PM
Hi all
I am trying to debug an issue at work where we use the LSM6DSV accel/gyro IMU chip and I am running into a little problem
The result registers for the accelerometer and gyroscope both say that they return a 16-bit two's complement result, and I get the following
| Gyro / Accel | Raw unsigned value (LOW | (HIGH << 8)) | Two's complement value (Signed) | Result (mG or mDPS) |
| Accelerometer X | 65524 | -12 | -0.732 |
| Accelerometer Y | 13347 | 13347 | 814.167 |
| Accelerometer Z | 111 | 111 | 6.771 |
| Gyroscope X | 32772 | -32764 | -143342.5 |
| Gyroscope Y | 32764 | 32764 | 143342.5 |
| Gyroscope Z | 37149 | -28387 | -124193.125 |
My system is sitting very still and on a somewhat level surface. The accelerometer seems correct. For a value close to 0, we see the unsigned value close to 0 or very high around 65535 which is what I would expect.
The gyroscope values for a zero rate I would expect to also be similar given the datasheet says this "The value is expressed as a 16-bit word in two’s complement"
My basic thinking is that these are expressed as a 15-bit word in two's complement.
I have double checked that the device is indeed an LSM6DSV chip as the WHOAMI register returned a value of 0x70
Just for additional reference, the gyro is configured in
high performance, 120Hz ODR and the sensitivity is set to 125 DPS
Any help would be much appreciated
Solved! Go to Solution.
2024-11-19 8:36 PM
I found the issue for this. It seems that the first reading from the gyro is junk. This wasn't the case for the accelerometer however.
2024-11-19 8:36 PM
I found the issue for this. It seems that the first reading from the gyro is junk. This wasn't the case for the accelerometer however.