cancel
Showing results for 
Search instead for 
Did you mean: 

configuring uart or swv on STEVAL-BCNKT01V1

Dinakaran Palani
Associate II

hi am planning to print the pcm buffer which is used in audio loop example but i am not able to configure the pins to print it on swd console or using uart

10 REPLIES 10

Hi @Dinakaran Palani​ ,

let me verify if I have well understood the point: you are able to read the audio stream on uart on your project, but you would like to merge it inside the Audio Loop example, is it? If so, can't you just substitute the USB function with the UART ones?

-Eleon