cancel
Showing results for 
Search instead for 
Did you mean: 

Change ODR on SensorTile

CRoma.11
Associate II

Hello,

I programmed the sensorTile STEVAL-STLKT0V1 with ALLMEMS1 end I used STM32CubeIDE with NUCLEO32.

How I can change the sampling frequency (ODR) of accelerometers and gyroscopes?

Thanks,

Chiara

12 REPLIES 12
CRoma.11
Associate II

Thank you very much for the useful advice. 

Best Regards,

Chiara

@CRoma.1​ 

you're welcome =)

just as a reminder, if you "select a best answer" in this thread you can help other community members with a similar question

Niccolò

DAlta.1
Associate II

Good Evening,

I have the same problem as Chiara. I would set a sample rate of 100Hz or higher. If I wanted to modify ALLMEMS1 firmware to do that (perhaps telling that from the app and saving results on the SensorTile SD ), how would I do?