2021-05-03 01:33 AM
Hello,
I programmed the sensorTile STEVAL-STLKT0V1 with ALLMEMS1 end I used STM32CubeIDE with NUCLEO32.
How I can change the sampling frequency (ODR) of accelerometers and gyroscopes?
Thanks,
Chiara
Solved! Go to Solution.
2021-05-04 01:47 AM
Thank you very much for the useful advice.
Best Regards,
Chiara
2021-05-04 01:50 AM
@CRoma.1
you're welcome =)
just as a reminder, if you "select a best answer" in this thread you can help other community members with a similar question
Niccolò
2023-04-03 09:01 AM
Good Evening,
I have the same problem as Chiara. I would set a sample rate of 100Hz or higher. If I wanted to modify ALLMEMS1 firmware to do that (perhaps telling that from the app and saving results on the SensorTile SD ), how would I do?