cancel
Showing results for 
Search instead for 
Did you mean: 

Cant initialize sensors ISPU getting started example

NicRoberts
Associate II

I'm working through the "Getting started with the X-CUBE-ISPU software package for STM32Cube" tutorial and trying the ISPU_Logging example.

NULCEO F411RE -> X-NUCLEO IKS02A1 -> STEVAL-MKI229AA (LSM6DSO16IS)

(This is also my first time using the Cube IDE so not sure where things are as its a different layout to the tutorial now)

I've set up the hardware pin outs & configured the software components for the appropriate sensors, generated the code, built & downloaded onto the board. The IDE says this was all successful...

File download complete

Time elapsed during download operation: 00:00:01.175

Verifying ...

Download verified successfully

 

I open up the Unicleo-GUI and am met with the following...

 

NicRoberts_0-1735824589251.png

So far so good, the board & its sensors have been recognized and that's the same sensors I added in the software component section

I click apply & ...

 

NicRoberts_1-1735824714192.png

 

What am I missing here? I've stepped through the document a few times now but cant for the life of me find what's missing

 

 

3 REPLIES 3
Petr S
ST Employee

Hello,

Could you please send me your ioc file for analysis?

Thanks and regards,

Petr

 

Actually please send me the whole project, I just realized you didn't generate it using CubeMX, right?

NicRoberts
Associate II

Thanks Petr - I've attached a zip of the project. Created in STMCubeIDE 1.17