2017-02-24 05:27 AM
Hi,
I'm working on the module SPSGRF-868 (868Mhz) connected to a PIC24F; the datasheet state that the maximum datarate for FSK is 500Kbps, but after a lot of test I can reach only 100Kbps with frequency dev of 32Khz, channel cut off filter at 200Khz and modulation FSK; every comunication test with data rate greater then 100Kbps and different modulation and freq deviation end with no comunication at all.
Is possible to achive a data rate of 250Kbps or more ?
Thanks.
#spirit12017-03-08 06:54 AM
Just an update, maybe should be useful.
Using a frequency deviation of 48Khz and a channel filter at ~260Khz the system is correctly working with datarate of 250kbps.