cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-H743ZI2

Sheraz2568
Associate II

Hello Everyone!

I think it's a weird question, however, I am new to NUCLEO-H743ZI2.  Actually, I am facing the issue of low-speed data transfer from MCU to PC (LabVIEW). Before, I was using programming and debugging USB ports to transfer data to LabVIEW. However, I was only able to transfer at a maximum of 115200bps (14400 Bytes ps). Although my requirement is 50,000 Bytes per sec. 

Then I found the USB OTG_FS Connector (CN13). However, I am not sure about the maximum speed through which I can transfer data. And what about the Ethernet port (CN14)? 

1 REPLY 1
TDK
Guru

The UART port should be capable of 921600 or more. Increasing baud rate is probably the easiest solution here.

USB FS can transfer around 5 Mbps, but is more complicated to program.

Eithernet faster than USB FS, unsure of the max but at least 10s of Mbps.

 

If you feel a post has answered your question, please click "Accept as Solution".