2018-02-17 2:45 AM
Hi,
I would like to debug a program on BlueNRG-1 using SWD interface on idb007v1 board.
Unfortunately, I cannot even program the chip via this interface.Here is my configuration:
1) ST-Link/V2 is connected by 20-lines ribbon cable to CN7 connector
2) idb007v1 board is powered from USB
3) ST-Link/V2 firmware version V2J30S7
4) Windows 7/64bit drivers:
a. STLink dongle 2017-06-08 v2.1.0.0 STMicroelectronics
b. VCP driver 2010-04-25 v1.3.1.0 STMicroelectronics5) IDE: Atollic TrueSTUDIO for STM32 9.0.0
When I try to start debugging in TrueStudio following error appears:
Atollic TrueSTUDIO gdbserver for ST-Link. Version 4.2.0 (WIN32 2018-01-16 10:57:14 15656)
Copyright (c) 2018, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistant Mode : Disabled
LogFile Name : debug_log.txt
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Vendor = 0x3B
Error in initializing ST-Link device.
Reason: ST-LINK: Could not verify ST device! Abort connection.
and sometimes:
Target no device found
Error in initializing ST-Link device.
Reason: No device found on target.
Just to verify programming ability via SWD I also tried to use ST-Link utility, it communicates with ST-Link/V2 but is not able to connect to device (i.e. chip).
Another flash programming tool - STM32CubeProgrammer does not support BlueNRG-1 chip.
I can only program BlueNRG-1 flash memory by BlueNRG Flasher.
But this tool is using another path based on preprogrammed bootloader and USART communication.I am interesting in using SWD and debugging feature.
How can I obtain that?
Kind regards,
Piotr#debug #idb007v1 #bluenrg-1 #truestudio #swd2018-02-17 1:00 PM
Small update, but not a solution of my problem:
BlueNRG chips have their ST-Link utility:
BlueNRG-1 ST-LINK utility for BlueNRG-1, BlueNRG-2 MCU
After instalation the tool has a SWD frequency set to 4MHz, so following error apears when I try to connect:
21:57:12 : Can not connect to target!
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
21:57:15 : No target connected
I needed to lower frequency to 100kHz to make it work with BlueNRG-1.
2018-02-20 3:11 AM
Have you tried asking on the Atollic forums?
2018-02-27 1:29 AM
This Is ok for programming the board, but not for the debug.
Did someone manage to debug an app on the IDB007V1 ?
2018-04-22 7:05 AM
Hi romaniuk,
Did you got any progress on this issue?
Are you able to work with Atollic TrueSTUDIO 9.00?
2018-04-23 7:57 AM
No.
Please read discussion on the Atollic Forum.It is still, not supported and they do not know when it will be.2018-09-15 9:20 AM
So disappointed....
I am using "Atollic TrueSTUDIO for STM32 9.0.1" with "BlueNRG-1_2 DK 3.0.0" + STlink-V2 for IDB007V2 (BlueNRG-2) board and having identical issue.
I tried IAR tools, result the same.
Anyone have ever success using STLink for debugging on BlueNRG-1,2 ??
2019-10-15 6:42 AM
Could not verify ST device!
Thank you so much, Kraal!
I inspected the looks of the chip and found it quite different from the ones I used before.
The text was not engraved but printed in a sloppy way. I think that your suggestion of a counterfeit is right.
I tried to make these counterfeits working under STM32CUBEIDE and OpenOCD.
Therefore, I adapted the st_scripts/target/stm32f1x.cfg file by replacing the 0x1ba01477 by 0x2ba01477.
I also added a line:
reset_config trst_only
This gives a error message:
Error: BUG: can't assert SRST
Neverthless, I could load and debug my code.
2019-10-24 8:41 AM
thanks a lot,
what exactly reset_config trst_only do?