cancel
Showing results for 
Search instead for 
Did you mean: 

How do I add filtered.c files using the WISE IDE?

elv.1
Associate II

I develop my projects based on BlueNRG-LP_LPS DK 1.2.0​,I open any demo and find that only part of the HAL driver is added to the link, but I need to use another driver and don't know how to add it ?

in the ​BlueNRG-LP_LPS DK 1.2.0\Drivers\Peripherals_Drivers\Src files,This is where all the HAL and LL drivers are stored:

0693W00000UokDGQAZ.png 

but in my project,Only a few have been added.0693W00000UokCcQAJ.png 

When I need to use another driver,such as rf_driver_hal_adc ,How do I add?

0 REPLIES 0