2025-03-25 3:27 AM
Hello,
I am encountering an issue when enabling the OpenAMP middleware in CubeMX for a new project targeting the STM32MP257F‑DK board. After creating the project and activating only the OpenAMP middleware (see attached screenshot), the build fails because several required files are missing. Below is the full error message generated during compilation.
Thank you in advance for your help.
11:12:24 **** Build of configuration Debug for project openAMP_mp257_CM33 ****
make -j12 all
arm-none-eabi-gcc "../OPENAMP/mbox_ipcc.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"OPENAMP/mbox_ipcc.d" -MT"OPENAMP/mbox_ipcc.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "OPENAMP/mbox_ipcc.o"
arm-none-eabi-gcc "../OPENAMP/open_amp.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"OPENAMP/open_amp.d" -MT"OPENAMP/open_amp.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "OPENAMP/open_amp.o"
arm-none-eabi-gcc "../OPENAMP/openamp_log.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"OPENAMP/openamp_log.d" -MT"OPENAMP/openamp_log.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "OPENAMP/openamp_log.o"
arm-none-eabi-gcc "../OPENAMP/rsc_table.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"OPENAMP/rsc_table.d" -MT"OPENAMP/rsc_table.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "OPENAMP/rsc_table.o"
../OPENAMP/mbox_ipcc.c:36:1: warning: "/*" within comment [-Wcomment]
arm-none-eabi-gcc "C:/Users/dn/STM32CubeIDE/workspace_1.18.0/openAMP_mp257/Middlewares/Third_Party/OpenAMP/libmetal/lib/system/generic/condition.c" -mcpu=cortex-m33 -std=gnu11 -g3 -DDEBUG -DUSE_FULL_LL_DRIVER -DCORE_CM33 -DUSE_HAL_DRIVER -DSTM32MP257Fxx -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -c -I../Core/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc -I../../Drivers/STM32MP2xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP2xx/Include -I../../Drivers/CMSIS/Include -I../OPENAMP -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Middlewares/Third_Party/OpenAMP/condition.d" -MT"Middlewares/Third_Party/OpenAMP/condition.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Middlewares/Third_Party/OpenAMP/condition.o"
36 | /* Includes ------------------------------------------------------------------*/
|
In file included from ../OPENAMP/mbox_ipcc.c:37:
../OPENAMP/openamp.h:25:10: fatal error: openamp/open_amp.h: No such file or directory
25 | #include "openamp/open_amp.h"
| ^~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [OPENAMP/subdir.mk:28: OPENAMP/mbox_ipcc.o] Error 1
make: *** Waiting for unfinished jobs....
In file included from ../OPENAMP/open_amp.c:21:
../OPENAMP/openamp.h:25:10: fatal error: openamp/open_amp.h: No such file or directory
25 | #include "openamp/open_amp.h"
| ^~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [OPENAMP/subdir.mk:28: OPENAMP/open_amp.o] Error 1
In file included from ../OPENAMP/rsc_table.h:23,
from ../OPENAMP/rsc_table.c:40:
../OPENAMP/openamp.h:25:10: fatal error: openamp/open_amp.h: No such file or directory
25 | #include "openamp/open_amp.h"
| ^~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [OPENAMP/subdir.mk:28: OPENAMP/rsc_table.o] Error 1
C:/Users/dnrfag/STM32CubeIDE/workspace_1.18.0/openAMP_mp257/Middlewares/Third_Party/OpenAMP/libmetal/lib/system/generic/condition.c:12:10: fatal error: metal/condition.h: No such file or directory
12 | #include <metal/condition.h>
| ^~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [Middlewares/Third_Party/OpenAMP/subdir.mk:88: Middlewares/Third_Party/OpenAMP/condition.o] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete.
11:12:26 Build Failed. 9 errors, 1 warnings. (took 2s.312ms)
2025-03-25 3:52 AM - edited 2025-03-25 3:53 AM
Hi @Nicolas_D ,
Thanks for your post. This is a known problem we are working on. BZ197530
We hope to provide fix in coming CubeMX release.
In the meantime you might take exemple on OpenAMP application exemple provided in CubeFirmware package and bring it in your project
Olivier
2025-04-10 4:43 AM - edited 2025-04-10 4:47 AM
Hi @Olivier GALLIEN ,
Thanks for your suggestion, I tried and fixed the same errors with STM32MP257F-DK, but a new problem appeared, the compiler did not find some macro as shown above.
Can you give me some ideas to fix them. Thank you very much.