cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I'm very new to STM32 and LCD RGB. Currently, I bought the LCD TFT AFY480272A0-4.3INTH. It says that the interface uses a 24-bit parallel RGB. Can I drive it using the NUCLEO-F767ZI? And, how do I connect the flexible cable to the Nucleo pin?

MSyai.1
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
2 REPLIES 2
MM..1
Chief II

Thanks, I'll order it soon. But I'm still confused about how to set the brightness on the Nucleo. The backlight has two pins, an anode and a cathode. The forward voltage of the backlight is 18V.0693W00000Y81KnQAJ.png0693W00000Y81MAQAZ.png