2024-06-27
03:42 AM
- last edited on
2024-06-27
04:47 AM
by
Lina DABASINSKAITE
I am using Vl53l8cx with stm32wb5mmdk. I am unable to initialize the sensor via this board. I used it with a nucleo board and it worked fine, but I need a BLE-based controller to share data.
SDA and SCL are pulled up with 4.7k 3v3 is connected to 5vo via voltage divider giving 3.3 volts , 1v8 is connected to 5VO via voltage divide giving 1.8 volts. SPI_I2c_N is connected to gnd pin.
All other connections are in the project file itself.
The link below will take you to the project file
2024-07-01 05:23 AM
I have tried all I could but have not been able to find the issue. I have configured LPUART instead of USART for trace related to BLE . Can this be a possible reason .
I need immediate help with this . It would be great if someone could give me even an idea of how it needs to be don.