2021-07-02 5:23 AM
Hello,
I'm trying to make the linux driver for VL53L3CX work on STM32MP157C-DK2. Already fixed some problems : made it work with new kernel by correcting functions names (timeval => __kernel_old_timeval and i2c_new_device => i2c_new_client_device , that's all), made it compile with bitbake and changed used gpio pins to use it on my board instead of raspberry pi.
The driver now compile. Also with i2cdetect -y 1 I verified that the VL53L3CX is connected and can be detected at adress 29.
But I have that error trying to load the kernel module :
modprobe stmvl53lx
result :
[ 545.281289] stmvl53lx_parse_tree: Unable to find boot-reg -22 41
[ 545.281366] get_pwren: pwren gpio disable
[ 545.291058] cci_read: i2c_transfer :-6, @29 index 0xe5 len 1
[ 545.299320] stmvl53lx_reset_release_i2c: boot fail with error -13
[ 545.299333] reset_release: reset release fail rc=-5
[ 545.310389] ------------[ cut here ]------------
[ 545.314976] WARNING: CPU: 0 PID: 1105 at drivers/regulator/core.c:2123 _regulator_put.part.0+0x164/0x16c
[ 545.324645] Modules linked in: stmvl53lx(O+) usb_f_rndis aes_arm u_ether aes_generic cmac algif_skcipher libcomposite snd_soc_audio_graph_card snd_soc_simple_card_utils brcmfmac stusb160x typec cfg80211 galcore(O) brcmutil stm32_crc32]
[ 545.377256] CPU: 0 PID: 1105 Comm: modprobe Tainted: G W O 5.10.10 #1
[ 545.384646] Hardware name: STM32 (Device Tree Support)
[ 545.389818] [<c0110824>] (unwind_backtrace) from [<c010c4e0>] (show_stack+0x10/0x14)
[ 545.397547] [<c010c4e0>] (show_stack) from [<c0b82f3c>] (dump_stack+0xb8/0xcc)
[ 545.404774] [<c0b82f3c>] (dump_stack) from [<c01249c0>] (__warn+0xec/0x104)
[ 545.411739] [<c01249c0>] (__warn) from [<c0b7e3fc>] (warn_slowpath_fmt+0x64/0xc4)
[ 545.419234] [<c0b7e3fc>] (warn_slowpath_fmt) from [<c067023c>] (_regulator_put.part.0+0x164/0x16c)
[ 545.428198] [<c067023c>] (_regulator_put.part.0) from [<c067026c>] (regulator_put+0x28/0x38)
[ 545.436771] [<c067026c>] (regulator_put) from [<bf285e38>] (stmvl53lx_release_gpios+0x2c/0xc8 [stmvl53lx])
[ 545.446451] [<bf285e38>] (stmvl53lx_release_gpios [stmvl53lx]) from [<bf286600>] (stmvl53lx_probe+0xb4/0xd4 [stmvl53lx])
[ 545.457263] [<bf286600>] (stmvl53lx_probe [stmvl53lx]) from [<c09242b4>] (i2c_device_probe+0x278/0x2b0)
[ 545.466611] [<c09242b4>] (i2c_device_probe) from [<c071d8ec>] (really_probe+0x208/0x4f0)
[ 545.474705] [<c071d8ec>] (really_probe) from [<c071dd9c>] (driver_probe_device+0x78/0x16c)
[ 545.482976] [<c071dd9c>] (driver_probe_device) from [<c071e0f0>] (device_driver_attach+0x58/0x60)
[ 545.491859] [<c071e0f0>] (device_driver_attach) from [<c071e1ac>] (__driver_attach+0xb4/0x154)
[ 545.500483] [<c071e1ac>] (__driver_attach) from [<c071b80c>] (bus_for_each_dev+0x78/0xc0)
[ 545.508673] [<c071b80c>] (bus_for_each_dev) from [<c071c964>] (bus_add_driver+0x170/0x20c)
[ 545.516944] [<c071c964>] (bus_add_driver) from [<c071ecdc>] (driver_register+0x74/0x108)
[ 545.525045] [<c071ecdc>] (driver_register) from [<c0924bc0>] (i2c_register_driver+0x3c/0xac)
[ 545.533560] [<c0924bc0>] (i2c_register_driver) from [<bf2868f0>] (stmvl53lx_init_i2c+0x34/0x108 [stmvl53lx])
[ 545.543397] [<bf2868f0>] (stmvl53lx_init_i2c [stmvl53lx]) from [<c01020c8>] (do_one_initcall+0x58/0x2bc)
[ 545.552835] [<c01020c8>] (do_one_initcall) from [<c01c4238>] (do_init_module+0x60/0x258)
[ 545.560933] [<c01c4238>] (do_init_module) from [<c01c6490>] (load_module+0x1434/0x1788)
[ 545.568945] [<c01c6490>] (load_module) from [<c01c6a6c>] (sys_finit_module+0xd4/0x130)
[ 545.576872] [<c01c6a6c>] (sys_finit_module) from [<c0100060>] (ret_fast_syscall+0x0/0x54)
[ 545.585050] Exception stack(0xcc0a5fa8 to 0xcc0a5ff0)
[ 545.590109] 5fa0: 00000000 00000000 00000003 0002270c 00000000 00040000
[ 545.598297] 5fc0: 00000000 00000000 00000000 0000017b 00034220 00000000 00000000 00000000
[ 545.606482] 5fe0: beb06890 beb06880 0001b3c9 410c8bb2
[ 545.611777] ---[ end trace c531c4ede0070016 ]---
[ 545.616597] stmvl53lx: probe of 1-0029 failed with error -1
Do anyone have an advice to help me in my research ? Where does that error come from ?
Thank you in advance
Solved! Go to Solution.
2021-07-26 3:57 AM
Hi @BJola.1 ,
The WARNING message in _regulator_put is caused by stmvl53lx_release_gpios called when stmvl53lx_setup fails (in stmvl53lx_probe).
But before that, an error has been returned by VL53LX_WaitDeviceBooted because chip didn't succeed to boot after reset.
[ 545.299320] stmvl53lx_reset_release_i2c: boot fail with error -13
Error -13 means VL53LX_ERROR_CONTROL_INTERFACE which is an error reported from IO functions.
Could you please share the device tree part related to stmvl53lx (especially xsdn-gpio pin) ?
Do you think you need to configure boot-reg ?
BR,
Christophe
2021-07-21 8:18 AM
Hi,
I'm not expert in SW, so take my answer with care.
Found some info about proximity sensors in https://wiki.st.com/stm32mpu/wiki/IIO_overview
(which is not exactly same reference, but hope it will help)
Regards.
2021-07-26 3:57 AM
Hi @BJola.1 ,
The WARNING message in _regulator_put is caused by stmvl53lx_release_gpios called when stmvl53lx_setup fails (in stmvl53lx_probe).
But before that, an error has been returned by VL53LX_WaitDeviceBooted because chip didn't succeed to boot after reset.
[ 545.299320] stmvl53lx_reset_release_i2c: boot fail with error -13
Error -13 means VL53LX_ERROR_CONTROL_INTERFACE which is an error reported from IO functions.
Could you please share the device tree part related to stmvl53lx (especially xsdn-gpio pin) ?
Do you think you need to configure boot-reg ?
BR,
Christophe
2021-07-26 5:47 AM
Hi !
Sorry, I wasn't able to answer last week.
Here is the dedicated par of my device tree :
&i2c5 {
status = "okay";
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
dmas = <&mdma1 36 0x0 0x40008 0x0 0x0 0>,
<&mdma1 37 0x0 0x40002 0x0 0x0 0>;
dma-names = "rx", "tx";
stmvl53lx: stmvl53lx@29 {
compatible = "st,stmvl53lx";
reg = <0x29>;
xsdn-gpio = <19>;
pwren-gpio = <12>;
intr-gpio = <16>;
};
};
dmas seems to come from a previous test. When I supress it, it seems to work.
I suppose the boot failed due to bad dma configuration.
Thank you for your help.
2021-07-27 12:41 AM
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'