2021-06-22 7:28 AM
2021-06-22 7:59 AM
This is the smallest ALS available in the market (Less than 2mm x 1mm), so really easy to integrate.
It came out on June 2021, all documentations are available on st.com, and product will be orderable starting mid-July 2021.
2021-06-22 7:40 AM
Welcome, @Community member to the community!
One of the highlights is the light flicker extraction, as mentioned in the datasheet:
With a patented architecture and a high-performance photodiode design, the VD6283
can extract light flickering frequencies to avoid “banding effects�? on videos, or check
that they are safe for human eye. Additionally, the VD6283 is the only sensor able to
extract different light flicker waveforms from 100 Hz and 2 kHz, including LED square
signals, that can run flicker operations simultaneously with ALS operations.
Does it answer your question?
Regards
/Peter
2021-06-22 7:59 AM
This is the smallest ALS available in the market (Less than 2mm x 1mm), so really easy to integrate.
It came out on June 2021, all documentations are available on st.com, and product will be orderable starting mid-July 2021.