cancel
Showing results for 
Search instead for 
Did you mean: 

Breakout Circuit for Satel-VL538

Rituraj
Senior

I am trying to use Satel -Vl53L8 after breaking it .  I am unable to operate it , I also tried to use the same method as used by brekout board but failed . Here is the circuit I used

Rituraj_0-1738560445285.png

Is there a way I can use the brakout board , What circuit do I need to use.

1 ACCEPTED SOLUTION

Accepted Solutions
Chihming
ST Employee

Hi User,

The connection of L8CX's breakout board is as the list.

Pin1-- AVDD; Pin2-- IOVDD; Pin3-- Core_1V8; Pin4-- LPn;

Pin5-- GPIO1; Pin6-- GPIO2; Pin7-- SPI_I2C_N; Pin8-- SCL;

Pin9-- SDA; Pin10-- MISO; Pin11-- NCS; Pin12-- GND;

You also can refer to the datasheet for connection of schematic. Please download following link.

Datasheet - VL53L8CX - Low-power high-performance 8x8 multizone Time-of-Flight (ToF) sensor 

The page7 you can find out all pins' definition. The page8 you can refer the schematic for connection.

Second, please make sure there are 2 power supply 1.8V and 3.3V.

Thanks,

Chihming

View solution in original post

1 REPLY 1
Chihming
ST Employee

Hi User,

The connection of L8CX's breakout board is as the list.

Pin1-- AVDD; Pin2-- IOVDD; Pin3-- Core_1V8; Pin4-- LPn;

Pin5-- GPIO1; Pin6-- GPIO2; Pin7-- SPI_I2C_N; Pin8-- SCL;

Pin9-- SDA; Pin10-- MISO; Pin11-- NCS; Pin12-- GND;

You also can refer to the datasheet for connection of schematic. Please download following link.

Datasheet - VL53L8CX - Low-power high-performance 8x8 multizone Time-of-Flight (ToF) sensor 

The page7 you can find out all pins' definition. The page8 you can refer the schematic for connection.

Second, please make sure there are 2 power supply 1.8V and 3.3V.

Thanks,

Chihming