Hi User,The connection of L8CX's breakout board is as the list.Pin1-- AVDD; Pin2-- IOVDD; Pin3-- Core_1V8; Pin4-- LPn;Pin5-- GPIO1; Pin6-- GPIO2; Pin7-- SPI_I2C_N; Pin8-- SCL;Pin9-- SDA; Pin10-- MISO; Pin11-- NCS; Pin12-- GND;You also can refer to th...
Hi Asha,ST provides sample codes for distance reporting and sample frequency. You should develop the direction and moving speed by yourself. Here is the link to the sample codes provided by ST.STSW-IMG040 - Ultra lite driver (ULD) API for the VL53L8C...