Skip to main content
videojames
Associate III
March 3, 2022
Solved

Calibration: Is it necessary if only the change in distance is the important value?

  • March 3, 2022
  • 1 reply
  • 916 views

In our application, we don't necessarily need to know the true distance, we only need to know when it's in a certain range, and it doesn't matter if that range is represented as 30-40mm or 50-60mm, only that is consistent.

Can we get away with not needing calibration if this is the case?

We are using a VL53L1X aimed through a IR transparent plastic.

This topic has been closed for replies.
Best answer by John E KVAM

I think it depends. If you build your system with a thin, clear, optically flat glass near to the sensor, then no, the effect of the crosstalk will not significantly affect your range at that distance.

But be a little careful. If you choose a big air gap between sensor and the glass, or the glass is of poor quality, then you could be in trouble.

The final determination of the quality of glass would be the calibration return. But with this sensor, if it works for you, it works. But the build-it-and-see-if-it-works can be expensive.

Buy the P-Nucleo-53L evaluation kit and test the glass you are using at your expected air gap. It will save you a lot of money in the long run.

Read and understand the article at:

https://community.st.com/s/article/Time-of-Flight-Cover-glass

And you will be fine.

  • john

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
March 3, 2022

I think it depends. If you build your system with a thin, clear, optically flat glass near to the sensor, then no, the effect of the crosstalk will not significantly affect your range at that distance.

But be a little careful. If you choose a big air gap between sensor and the glass, or the glass is of poor quality, then you could be in trouble.

The final determination of the quality of glass would be the calibration return. But with this sensor, if it works for you, it works. But the build-it-and-see-if-it-works can be expensive.

Buy the P-Nucleo-53L evaluation kit and test the glass you are using at your expected air gap. It will save you a lot of money in the long run.

Read and understand the article at:

https://community.st.com/s/article/Time-of-Flight-Cover-glass

And you will be fine.

  • john
If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.