Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L5CX Motion Detection (vl53l5cx_plugin_motion_indicator) does not appear to update sensor for vl53l5cx_motion_indicator_init and vl53l5cx_motion_indicator_set_resolution data initializations and changes

The functions  vl53l5cx_motion_indicator_init  and vl53l5cx_motion_indicator_set_resolution rely on code in vl53l5cx_motion_indicator_set_resolution to update the sensor settings. However, the code only executes if an error is encountered prior to th...

DHrynyk by Associate
  • 1807 Views
  • 2 replies
  • 0 kudos

How does a VL53L0X react with multiple targets in FOV

I understand that there are models with multiple zones, but what I am trying to figure out is how a single zone TOF sensor will react when inside the FOV there are multiple targets.For example - if there is a wall at 100cm covering the full FOV, but ...

DOelk.1 by Associate
  • 1599 Views
  • 1 replies
  • 0 kudos

Cover for TOF sensors

Hi Community,I'm doing some experiments with the VL53LXX-V2 sensorI would need to find a cover glass for this sensor with the divider to avoid crosstalk.I can't find it on the market and I can't contact HornixWhere else can I find it?Thank youBest re...

FLa G.1 by Associate
  • 1412 Views
  • 2 replies
  • 0 kudos

VL53L1X in a tube.. Tips and tricks?.

I like the VL53L1X because the ROI is narrow, and I have seen other posts about a TOF in an opaque tube, but have a few questions still. I get that the beam can be narrowed to 15 degrees, and I have seen that the suggestion is to use matte black i...

CBarr.3 by Associate
  • 1779 Views
  • 1 replies
  • 0 kudos

Initialisation of the VL53L5CX failed.

Hi, I read the question from 'Peter': VL53L5CX driver vl53l5cx_init() fails in the forum and wonder if downloading the firmware was successful. I am using a Rasberry Pi and used the Unosquare.WiringPi, C#.There is no methode to write multiple bytes, ...

BPutt.1 by Associate II
  • 1396 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L5CX Offset Calibration

Hi,I noticed that an offset calibration function is missing in the API of the VL53L5CX (like seen before on VL53L1CX). Only the xtalk calibration is available.Is this because all the VL53L5CXs are individually factory offset-calibrated?My assumption ...

MFabb.1 by Associate II
  • 2330 Views
  • 2 replies
  • 0 kudos

Error Message after Start VL53L1X_GUI "Ranging Sensor Failure" ..."SciChart.Chartig3D..SciChart3DSurface" ... Exception

I have Problems to Start the VL53L1X_GUI (STSW-IMG0081.0.0 - R10647), after Installation on different "Win 10 Pro 21H2"-Systems, with or without plugged target board, the error message is always the same: "Ranging Sensor Failure" by calling the c...

JEich.1 by Associate
  • 1516 Views
  • 3 replies
  • 0 kudos