Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L8CH GUI

Hello,I am interested in the ToF-Sensor VL53L8CH to get access to the histogram data. Is there any Evaluation-GUI to easily try out this sensor and to see the histogram data, similar to the GUI for the VL53L8CX (STSW-IMG041 - VL53L8CX Demo GUI)?Thank...

PhKE by Associate
  • 1823 Views
  • 2 replies
  • 1 kudos

Resolved! VL53L0X: How to narrow the FOV

Greetings Team,Have a question (that may not be so quick). Currently working on a project where I need to detect a tube's length, using the VL53L0X, from ~30 to 200mm. The problem is that the inside dimensions of the tube are 20x11mm, quite tight. I'...

JOsbo.1 by Associate
  • 5239 Views
  • 5 replies
  • 1 kudos

Resolved! How to properly drive the VL53L0X into Sleep mode?

The datasheet mentions putting the sensor into sleep by driving XSHUT low. measuring the power consumption shows that the power is consumed more when I connect XSHUT even when I drive it low by 200 microAmp. The XSHUT is normally pulled-up on the bre...

AElgh by Associate III
  • 8598 Views
  • 14 replies
  • 1 kudos

gesture library in STSW-IMG035

Hello! I am an undergraduate student interested in gesture recognition based on ToF ranging sensors. How to use the gesture library to train a model for the STM32CubeMX project?Is there a tutorial? If possible, could you provide the complete project ...

VL53L3CX with Atmega328pb Xplained Mini

Hi,I am using the VL53L3CX distance sensor for a project and I am wondering if it's possible to create my own library functions. The MCU I am using is the ATmega328PB XPlained Mini from Microchip, which only has 32KB of flash memory. The API library ...

castor by Associate
  • 1947 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CX temperature update

Hi,I was wondering if someone can help me with temperature update on the VL53L4CX.According to UM2931  that describes the temperature update in paragraph 3.5 there is a dedicated function named VL53L4CD_Start_Temperature_Update() and can be used when...

Gabor23 by Associate II
  • 5954 Views
  • 6 replies
  • 1 kudos

Resolved! VL53L5CX Power Consumption

Hello @John E KVAM ,Table 14 in the datasheet shows power consumption in Autonomous as going as low as 4.5 mW, but is this only the AVDD power? or total device power? Because I do measure low power draw at those levels, but only on the AVDD pin (and ...

DBonh.1 by Associate III
  • 7081 Views
  • 8 replies
  • 0 kudos

VL53L8 smalles FoV

Hi,I have a project for which I need to measure a tank level of tanks with a maximum depth of 3 meters. The challenging part is that many tanks have filling tubes with an inner diameter of 50mm but a length of 1000mm worst case. I have made this draw...

bitmap.png
daan by Associate II
  • 2140 Views
  • 2 replies
  • 0 kudos