Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L5CX platform code using Raspberry Pi Pico

Hi there,I'm currently trying to write the platform code for the VL53L5CX using a Raspberry Pi Pico.I'm trying to publish the sensor data via micro-ROS in a ROS2 topic. When I use my current code I only get values close to zero and they are the same ...

vinc00 by Associate
  • 2442 Views
  • 1 replies
  • 1 kudos

Resolved! Maximum distance limit in VL53L1X

HiI want to use the VL53L1X to measure the distance of a target less than 30 cm away and about 1 cm in size.Is it possible to ignore the measurements above 30 cm?I would like to know the settings to ignore the area above 30 cm when calculating a dist...

kbsh by Associate
  • 2013 Views
  • 3 replies
  • 0 kudos

We are looking for a TOF sensor that meets some requirements

Moved  from the Feedback forum - which is not for product questions.Dear person in chargeCould you please reply to the following?Thank you so much for your attention and participation.Q1We are looking for a ToF sensor that meets the following require...

KF1 by Associate
  • 1581 Views
  • 2 replies
  • 1 kudos

Resolved! VL53L0X API download

Hello, I faced *** problem because of *** website and can't download VL53 range sensor API.It may be that I'm *** as well. But every time this *** button does nothing: https://www.st.com/en/embedded-software/stsw-img005.html#st-get-software   So ST ...

ST_Lovemachine_0-1737493778802.png

Resolved! Can a TOF sensor detect a person through a plastic case?

HI We are thinking about a method for detecting people.   The prerequisite is that we need to detect people by penetrating a plastic case with a thickness of about 3mm (white). The existing PIR cannot penetrate the case, and radar sensors are expensi...

moon1003_0-1736746444564.png
moon1003 by Associate III
  • 2619 Views
  • 3 replies
  • 3 kudos

Resolved! VL53L1X and VL53L4CD GetSensorId

Following up on a diff post.  I have a strange result. If I call the GetSensorId for the VL53L1X we use today I get a return of decimal 61098 which is 0xEEAA.  However the comments in the code claim for the GetSensorId should be: "This function retur...

will3 by Associate III
  • 2626 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L1X and VL53L4CD detection

We are beginning to migrate from the L1 to the L4.  Wondering if there is a way to auto-detect which sensor is on the board? I would like to build one fw version which abstracts away which sensor is in use (albeit taking advantage of diff features) b...

will3 by Associate III
  • 1912 Views
  • 2 replies
  • 0 kudos

Resolved! ToF sensor with highest sampling frequency

In the search for a distance senor which can sample at highest rate. Given the constraint of a measurement range <1m and accuracy of relative distance changes in the low mm range. Ideally we could get a sampling rate of 1kHz.The VL53L4 sensors would ...

Tom_pm by Associate III
  • 2881 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L1X when to trust readings?

Hi,   typedef struct { uint8_t Status; /*!< ResultStatus */ uint16_t Distance; /*!< ResultDistance */ uint16_t Ambient; /*!< ResultAmbient */ uint16_t SigPerSPAD;/*!< ResultSignalPerSPAD */ uint16_t NumSPADs; /*!< ResultNumSPADs */ } VL53L1X_Result_t...

will3 by Associate III
  • 1795 Views
  • 3 replies
  • 2 kudos