Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

在同一条i2c总线轮询使用两个vl53l1x出现只有一个有反应的问题

这是我的代码,我之前以前改地址成功了的,这里就开始测量数据while (1) {        // 获取当前时间作为起始时间        clock_gettime(CLOCK_MONOTONIC, &start_time);  // 获取起始时间                for (i = 0; i < 2; i++) {  // 轮询两个传感器            Timeout = 0;            dataReady = 0;            // 检查数据是否...

QQ截图20250206165222.png
eneeen by Associate II
  • 3564 Views
  • 6 replies
  • 0 kudos

STM32 Smart Presence Detection VL53L8X

Hi,Im currently testing the Smart Presence Detection Firmware for the VL53L8X and have some questions:- When I start the ranging, the firmware triggers false positives (detecting someone when there isn't anyone) and after some seconds it stabilizes t...

MikeReg by Associate II
  • 1512 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L8CX SPI communication

Hi all,I'm trying to setup the SPI communication with a VL53L8CX which is connected to a STM32F401RE-Nucleo. I took some code snippets from the STSW-IMG040 package and I wonder why the bytes to be send in VL53L8CX_WrMulti and VL53L8CX_RdMulti are tre...

bastl by Associate
  • 893 Views
  • 1 replies
  • 1 kudos

Resolved! VL53 as a reflectometer

Hi,I want to create a reflectometer to measure samples targets reflectivity in %. The samples are 10x15cm and the distance will be fixed: samples can be between 15cm to 1m. The measurement will happen in the dark in a controlled environment.I found t...

sensor model VL53L1X

Subject: Request for Technical Information and Quotation – Sensor Testing for Precision Seeding Applications Dear Mr , My name is Giovanni Ziliani, and I am an expert in industrial automation and sensor technologies. I currently provide specialized c...

Resolved! EMVA1288 Datasheets

I am exploring STM image sensors for a new project and am evaluating different options. To make an informed decision, I would like to refer to EMVA1288 datasheets, especially for details on read noise and dark current performance. Could you please le...

Resolved! VL53L7CX SDA stuck at zero

Hi, I am testing the SATEL VL53L7CX board, but the SDA on this board is stuck at zero. I have checked that there are no short cuts and that the pull up is there. Any ideas how to solve this?

Resolved! The interrupt of VL53L4CD cannot be used

I found a problem while using the VL53L4CD. My usual practice is to initialize the VL53L4CD after the terminal is turned on. During subsequent use, I only use Start and Stop to control whether to start ranging.Now it is found that when I stop, the te...

Blue666 by Associate II
  • 3594 Views
  • 9 replies
  • 0 kudos