User Activity

I use a VL53L3 with the STSW-IMG033 Ultra Low Power API. I use the settings in the settings mentioned in AN5769 "Using the VL53L3CX under ultralow-power mode" for maximum detection under daylight: Full ROIMacro period 200Signal limit 1500Sigma limit ...
I have an STM32 Nucleo F401RE plus X-Nucleo-53L3A2 board.IDE and the rest of the toolchain installed, including the STSW-IMG016 P-NUCLEO-53L3A2 pack graphical user interface.The data brief of the GUI states "I2C transaction recording" which is of my ...
Kudos given to