2024-12-16 3:14 AM
Hello.
I am designing a product using the VL53L7CH model.
I am using a 3.3V MCU.
So I'm trying to use 3.3V for both IOVDD and AVDD's voltage level.
Is there no problem if I use the same line without distinguishing IOVDD and AVDD?
Regards,
KORM
Solved! Go to Solution.
2024-12-16 7:37 AM - edited 2025-01-02 11:25 AM
That is absolutely fine. A bit of care not to exceed the max voltage would be recommended. But it will be very happy running at 3v3 for both the AVDD and the IOVDD.
- john
2024-12-16 7:37 AM - edited 2025-01-02 11:25 AM
That is absolutely fine. A bit of care not to exceed the max voltage would be recommended. But it will be very happy running at 3v3 for both the AVDD and the IOVDD.
- john