Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Current consumption vs supply voltage VL53L0x / VL53L1

Hy,I need to design a power consumption optimized (battery based) system using the VL53L0x / VL53L1. I cannot find the current consumption vs voltage in the datasheets. I can either use battery voltage directly (3.6V) or use a high efficiency DCDC (i...

harald by Associate III
  • 2277 Views
  • 3 replies
  • 0 kudos

Why does VL53L1X full API take up SO much memory?

So I am working with a VL53L1X sensor on a LPC804 from NXP. I am using the full API (STSW_img007). I made a simple test to see if I could get the I2C functions running allright, so I tried to read out the model ID. When I was successful, I wanted to ...

VL53L1X Setting up roi on the raspberry pi

Hey there,I just got the sensor working on my raspberry using the library I found online. The sensor can now measure the distance.Now for my schoolproject I need to setup 2 roi regions on the VL53L1x. I have searched the internet and cant find anythi...

VL53L1X: calibration flow

Hello,I have a question regarding the calibration flow. I have narrowed the RoI to my needs and adjusted the timing/intermeasurement budget and I am using short distance mode.My question now is whether I have to use the same settings when calibratin...

DZyla by Associate
  • 1221 Views
  • 2 replies
  • 1 kudos

What are vl53l0x functions and how do I add to stm32f1?

I want to add this sensor to stm32f1 https://pt.aliexpress.com/item/33036852017.html?src=google&albslr=222492145&src=google&albch=shopping&acnt=494-037-6276&isdl=y&slnk=&plac=&mtctp=&albbt=Google_7_shopping&aff_platform=google&aff_short_key=UneMJZVf&...

Resolved! VL53L1X: what is the difference between 2V8 and 1V8 mode

To use the VL53L1X with a 3V3 supply, I will have to select 2V8 mode.The default mode is 1V8 mode. The selection wil be done in 1V8 mode. Apperently I2C will function correct in 1V8 mode with a 3V3 supply.What is the difference between 1V8 and 2V8 mo...

PSimo by Associate
  • 2188 Views
  • 1 replies
  • 0 kudos