Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L5 Thresholds

Is there any documentation how to setup the various threshold parameters? These are the macros defined in the vl53l5cx_plugin_detection_thresholds.h#define VL53L5CX_DISTANCE_MM            ((uint8_t)1U)#define VL53L5CX_SIGNAL_PER_SPAD_KCPS      ((uin...

BBald.1 by Associate II
  • 1801 Views
  • 3 replies
  • 0 kudos

VL53L1 returns 65XXX values

I have multizone ranging mode enabled along with SHORT distance mode.I am getting a lot of readings with 65XXX values, for example:[8191, 65277, 65243, 65257, 65312, 65267, 65238, 65168, 65241, 65263, 65239, 65211, 65227, 8191, 65217, 65173, 65244][8...

VL53L5CX Examples (9 & 11) using interrupt

I'm using a X-NUCLEO-53L5A1dev board that I have wired up to a Raspberry Pi. I have also wired the interrupt line from dev board (cn-8 pin 3) to the Raspberry Pi GPIO1 (pin 28 on the 40 pin header). In the examples 9 and 11 there is a dummy functio...

BBald.1 by Associate II
  • 1168 Views
  • 1 replies
  • 0 kudos

Resolved! Issues while interfacing two VL53L1X sensors using Esp32

Hi ST team and community!I am trying to develop a People Footfall Counter for commercial use using the two VL53L1X Sensors on Esp32 using the Sparkun Library from the following:https://github.com/sparkfun/SparkFun_VL53L1X_Arduino_LibraryFirst of all,...

PNadar08 by Associate II
  • 5846 Views
  • 4 replies
  • 0 kudos

Resolved! Having trouble getting the stm vl53lx driver working on RPI

Hi - I can't seem to get the driver to compile on a RPi 3+..Grateful for any assistance !! This is the error message I get: pi@raspberrypi:~/VL53L3CX_LinuxDriver_1.0.5_bare_1.2.4/driver/vl53Lx $ make VL53LX_FULL_KERNEL=1CONFIG_STMVL53LX=m make -C /li...

DCamp.5 by Associate II
  • 2922 Views
  • 5 replies
  • 0 kudos