Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L5CX-SATEL and Rpi Linux Driver Build failure?

Hi, I am trying to build the user mode linux driver on my raspberry pi 4 for the VL53L5CX module, and when I follow the instructions in the guide for RPI, I cd into user/test and make, I get the following error:../uld-driver/src/vl53l5cx_api.c: In f...

VBhat.1 by Associate III
  • 2322 Views
  • 3 replies
  • 1 kudos

Resolved! VL53L5CX not showing up correctly on i2cdetect raspberry pi

Hi, I have followed the instructions in the PDF "VL53L5CX_Linux_Getting_started_with_Rpi.pdf" from the VL53L5CX linux driver, and I have built the program. I am having an issue now seeing the TOF sensor when I connect the VL53L5CX-SATEL board to the ...

VBhat.1 by Associate III
  • 2628 Views
  • 2 replies
  • 1 kudos

How to use VL53L5CX-SATEL assembled with X-NUCLEO-53L5A1

Hi,When I use only X-NUCLEO-54L5A1 (Expansion board with VL53L5CX), VL53L5 GUI is connecting to X-NUCLEO-VL53L5A1 well.However, when I plug-in VL53L5CX-SATEL board to the LEFT, RIGHT or both connectors, VL53L5 GUI can't be able to connect to X-NUCLEO...

WOh.1 by Associate II
  • 1993 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L5CX GUI shows no list of VL53L5CX.

I purchased P-NUCLEO-53L5A1 including X-NUCLEO-53L5A1 and NUCLEO-F401RE.And I assembled them and connect to PC, and then I installed its driver and reboot windows 10.When connecting, the explorer open the mass storage drive (D: (F401RE)).However, VL5...

0693W00000Dq4uZQAR.png
WOh.1 by Associate II
  • 2467 Views
  • 3 replies
  • 2 kudos

VL53L5CX mutual influence of multiple sensors

In some of our products we are using VL53L1 sensors. During evaluation, we figured out that there is an effect of mutual influence between multiple sensors measuring simultaneously (especially when using the histogram based measuring approach of the ...

mf101 by Associate II
  • 2035 Views
  • 3 replies
  • 0 kudos

Unable to communicate to VL53L0CX

Working on a board that uses a VL53L0CX. But I do not seem to be able to communicate with the sensor and have even tried to scan i2c addresses with no luck. I am hoping someone here can take a look at the schematic I have for the sensor and let me kn...

0693W00000Dm0tYQAR.png 0693W00000Dm0sBQAR.png
CBoyc.1 by Associate II
  • 2316 Views
  • 4 replies
  • 0 kudos

VL6180_SimpleRanging example using Bottom sensor

I'm trying to adapt the example code available on st.com for VL6180_SimpleRanging (STM32CubeExpansion_6180A1_V1.0.0 for STM32F401RE-Nucleo) so that the Bottom sensor is used, rather than the one soldered directly on the 6180XA1 expansion board (V2).M...

DHess.1 by Associate II
  • 2022 Views
  • 2 replies
  • 0 kudos