Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Does the VL53L1X GUI work?

I'm using the X-NUCLEO-53L1A1 and the STM32F401. As the user manual suggests. The GUI opens, but cannot detect the sensor. "Sensor Not Detected. Please ensure sensor connected then Press Black Reset Button on the Nucleo". The X-NUCLEO-53L1A1 is seate...

DAzu.1 by Associate II
  • 1957 Views
  • 2 replies
  • 0 kudos

Resolved! VD6283 GUI Communication Errors

In order to test the X-NUCLEO-6283A1 I installed its GUI (en.VD6283_Setup_v1.0.0.exe).I also installed the ST Link USB driver (as suggested in the GUI Guidelines) and the board is correctly recognized by the host. The GUI seems working fine the very ...

0693W00000FDGuaQAH.png 0693W00000FDH1vQAH.png 0693W00000FDH2pQAH.png 0693W00000FDGzpQAH.png
MFabb.1 by Associate II
  • 3374 Views
  • 6 replies
  • 0 kudos

Very unstable operation of the VL53L0X sensor. It can output 8191/8190 on the first run and output correct values on the second. Please any suggestions how to solve the problem?

Hello. I have problems with VL53L0X sensor. I will list my observations here.First, I carry out the calibration procedure. The sensor passes all initialization steps correctly (Data Init(), Static Init() and so on). Then calibration is performed. For...

histograms with two peaks when detecting a single target

We are using VL53L3CX evaluation board to dig out some information from the histogram.The 24-bin histogram are retreived by calling the Get_AdditionalData function. Two consecutive sets of histograms are got, when we use a white wall as target and th...

0693W00000GY6xLQAT.png
旭王.1 by Associate II
  • 1729 Views
  • 2 replies
  • 1 kudos
JYoon.5 by Associate II
  • 2398 Views
  • 4 replies
  • 0 kudos

VL53L5CX API Size "vl53l5cx_buffers.h" seems to be too large for the MCU to handle. Is splitting the buffers ( "VL53L5CX_FIRMWARE[]" )into smaller 'chunks' to send to the SPAD a reasonable solution?

I am trying to use the VL53L5CX with an AVR128DB48. The .h file "vl53l5cx_buffers.h" seems to be too large for the MCU to handle. I think, as it stands, it breaks the 32727 byte limit that AVR is capable of. Is splitting "VL53L5CX_FIRMWARE[]" into sm...

DAzu.1 by Associate II
  • 2285 Views
  • 4 replies
  • 0 kudos