2025-02-25 12:48 AM
Hello,
i'm using VIC3DA module in a dashboard to measure the vehicle speed. I encountered 2 big issues.
1. Some times the module requires several minutes to fix the position, even in warm start
2. Some times the speed coming from the module in completely random even if the vehicle is at 0 km/h of speed.
In that conditions, if i turn-off and on again the power supply, some times the module starts to works normally and fix the satellite in a reasonable time (<=1 min).
I read a document about the IMU calibration. Is it really required? Since i'm working for an automotive project, will be quite impossible to calibrate every dashboard after the production, because of the big amount.
Are there any special settings to do on the module to improve time to fix and sensor fusion function?
Many thanks