2018-09-27 03:45 AM
2018-11-07 01:56 AM
7 44
2018-11-08 12:49 AM
Ciao Francesco, Karim
The module in your hands isn't the final one.
It's a prototyping sample built in ~Nov 2017.
On board there isn't the final firmware.
We could plan a firmware-update of the module to promote the module to the final firmware.
@Francesco, On which board are you testing the module?
Thanks
Ciao
Francesco
2018-11-08 01:49 AM
Ciao Francesco and Karim,
The module is on a proprietary testing board. Here below the FW versions:
OS20LIB_4.3.0_ARM
GPSAPP_2.4.0.1_ARM
BINIMG_4.6.8.1_ARM
SWCFG_8204941a
WAASLIB_2.20.0_ARM
STAGPSLIB_5.1.0_ARM
STA8090_622bc043
GNSSLIB_8.4.10.16.3_ARM
Can I update the firmware by myself using the tool STA808x/9x Firmware Upgrade?
Where can I download the bin file?
Best regards
Francesco
2018-11-08 01:55 AM
Ciao Francesco
> Can I update the firmware by myself using the tool STA808x/9x Firmware Upgrade?
if in your board you can reset the module (just with a simple push-button or similar..) yes you can.
> Where can I download the bin file?
We will send the binary by email.
Is it ok?
Thanks
Ciao
Francesco
2018-11-08 02:25 AM
Ciao Francesco,
I can force the Reset pin to a low level (pin9 - SYS_RESETn) as described in the manual: "When the user wants to update the Teseo-LIV3F, Teseo-LIV3F must be powered and under reset; the user must configure the tool, select binary image and start firmware upgrade process. Only when the process has started, user must take Teseo-LIV3F out of reset."
Thank you, Francesco and Karim.
Francesco
2018-11-08 02:59 AM
Ciao Francesco
Perfect! You already have what you need ;-)
You can go ahead with firmware-update.
Let us know.
Ciao
Francesco
2018-11-08 05:28 AM
After the upgrade, now it is working as I expected.
Great.
Thank you very much!
Francesco
2018-11-08 05:31 AM
Ciao Francesco
Perfect.
Let us know if the 4 hours issue is still there.
Thanks
Ciao
Francesco
2018-11-14 03:12 AM
Ciao Francesco,
I made several tests and Teseo, with the FW update, is working: it receives GPS and GLONASS.
I have one more question: how can I receive GALILEO satellite? Is there a configuration/enable?
Teseo-Suite require an activation key to unlock some feature, how can I have that?
Ciao
Francesco
2018-11-14 04:49 AM
Ciao Francesco
To enable Galileo you have to reconfigure the module.
Have a look into the attached presentation (slide 7) where all the possible configurations are listed (with related command).
For Teseo-Suite you can ask activation key to the Teseo-suite support.
Hope this help
Ciao
Francesco