2020-10-12 4:03 PM
2020-10-13 12:41 AM
Hi.
You are right, I'l take note to fix it in the next version:
FYI:
0; Constellation disabled;
1: Constellation satellites only tracked;
2: Satellites constellation used in position evaluation
Regards
Francesco
2020-10-13 4:48 AM
Ok Tks
may be an error page 192/239 "Enable/disable the usage of RTC from the GNSS engine. It is recommended to have RTC
usage disabled (Bit12 set to 1) is the RTC crystal is not mounted"
should be (Bit12 set to 0) if disabled or 1 if enabled