GNSS positioning

Ask questions and find answers on Teseo GNSS positioning solutions. Discuss NMEA sentences, SBAS activation, and signal troubleshooting.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Dead Reckoning on ISM330DHCX

Hello, Does ISM330DHCX support Dead Reckoning like ASM330LHH?If yes, can we load the Dead reckoning firmware on X-STM32MP-GNSS2 with the ISM330DHCX module?

Resolved! Teseo-LIV3FL support for NAVIC (IRNSS)

Hello, We propose using Teseo-LIV3FL to design a new product. This part is selected because it supports Differential GPS (SBAS) and Real-time AGNSS.Please let us know if LIV3FL supports NAVIC (IRNSS). If not, can we upgrade the firmware to support NA...

Resolved! STA8100 NMEA Data Flow Filter

Hi,Currently using the STA8100_MF_DRAW_Binary_Image_v5_9_22 firmware, could you demonstrate commands to specify the received NMEA data streams, such as $GPGSV, or commands to disable all data streams & control the output frequency? It would be great ...

chriswu by Associate
  • 1011 Views
  • 2 replies
  • 0 kudos

Taseo-LIV4F Firmware Upgrade for NavIC

While upgrading Taseo Firmware for NavIC through UART interface to PC, I got the following error message:Upgrade command errorPlease check software baud rate or select recovery modeMy setting are:Loader baud rate: 115200Software baud rate 115200Jumpe...

TESEO LIV3F: Antenna RF path

Hi,I just designed a pcb with LIV3F module. I tried to follow layout instructions but I'm not RF expert. I can read through the USART bus but every values (GPGGA, GPVTG, etc.) are set to 0, as if there is no input RF signal. Herein below schematic de...

vin883_0-1727810856124.png
vin883 by Associate II
  • 2935 Views
  • 9 replies
  • 0 kudos

LIV4F-ME Firmware Documentation

Thanks for the info and the code snippets in this thread. However, they aren’t as good as proper documentation. Will the LIV4F docs get an update to include all of the LIV4FM / ME firmware details?   Related thread: https://community.st.com/t5/gnss-p...

WiFiLuke by Associate II
  • 1579 Views
  • 6 replies
  • 1 kudos

GPS data being sent vs Teseo Suite

Hello all,   I have a GNSS1A1 board with the LIV3F module. My problem is, in teseo suite my gps location shows up accurately, however when I look at the messages it is clear to me my location in those messages are far away from me.How is this possibl...

gamelk by Associate III
  • 640 Views
  • 1 replies
  • 1 kudos

Resolved! PROBLEM WITH X-NUCLEO-GNSS1A1 and NUCLEO-F446ZE

Hi I have connected the GNSS1A1 board and F446ZE boards. When I run the FW (Virtual Com Port) that I set up through STM32CUBE IDE (X-CUBE-GNSS) and start the program, when it enters MX_GNSS_Process() the gnssMsg struct's buffer pointer is pointing at...

bufatreserved.png bufatreserved.png bufatreserved.png
gamelk by Associate III
  • 4292 Views
  • 20 replies
  • 1 kudos

teseo vic3da does not update location

Hi, I bought a TESEO VIC3DA from MIKROE some time ago. I am addressing it via UART. I am receiving RX data, but it is always the same. The same location is always returned. I can also see in the frame that I have 0 satellites. However, I had the hard...