Subject | Author | Posted | |
---|---|---|---|
I use Internal comparator trigger Timer etr function to impelement cycle-by-cycle current mode cont...
| 2022-11-27 7:31 PM | ||
hi any one can help how to got sorce code stm32f334 for full bridge i need for design 10kw sic dc...
| 2022-11-24 11:00 PM | ||
Hi, I am using a Nucleo F401RE and a X-Nucleo-IHM07 shield for motor control applications. I am sup...
| 2022-11-23 8:34 AM | ||
I have been looking into using feed forward for a project that requires a relatively high speed (~1...
| 2022-11-19 12:58 AM | ||
I have custom design PCB using STM32F302CBT6 as bldc motor speed controller with back emf. Half of ...
| 2022-11-18 8:45 AM | ||
I am a newer leraning motor FOC control. I study the generated code by MCSDK tool with hall (120 d...
| 2022-11-16 5:25 PM | ||
Hi, I have a STEVAL-SPIN3204 board. I have opened the 6step_steval_spin3204 project on the ST moto...
| 2022-11-15 9:26 AM | ||
Hi there, I'am using STEVAL-SPIN3201 evaluation board. I've reset PA11 for overcurrent output si...
| 2022-11-13 10:22 PM | ||
Hey @ all the setup: custom motor control PCB microcontroller: STM32G431CBU6 gate-driver: U...
| 2022-11-10 1:06 AM | ||
I'm working on a project whith use a STM32F407 MCU to control a bldc motor and also has a low power...
| 2022-10-17 6:13 PM | ||
Hi I need to control a stepper motor with TMC2209 driver from my STM32G4 project but I cannot f...
| 2022-10-11 4:47 AM | ||
Hello community! I am using a custom PCB based on STM32G431CBU6 with external lowside current sen...
| 2022-10-05 4:27 AM | ||
Hello, Actual behavior: While I have deactivated the overvoltage protection in Motor Control Wo...
| 2022-09-27 6:51 AM | ||
I am using the STEVAL-ESC001v1 board to control a brushless motor. The project is started with Mot...
| 2022-09-26 9:39 AM | ||
Hi, I am trying to run a brushless motor at constant speed and at a ramped input (from 0 rpm to ...
| 2022-09-22 1:24 AM | ||
Hello, I am working on a project that requires control the motor speed by adjusting bus voltage. Th...
| 2022-09-20 8:27 PM | ||
Trying to use B-G431B-ESC1 - Discovery kit with specific motors, Rs = 0.1 om, Ls =0.01 mH. STM Moto...
| 2022-09-19 2:19 PM | ||
I've got an X-NUCLEO-IHM03A1 (the PowerSTEP based board) and a NUCLEO-G431RB. I'd like to start on ...
| 2022-09-10 7:42 PM | ||
We are using STM32F301 micro along with 5.4.4 motor control SDK. We found that at different speeds ...
| 2022-09-05 1:38 AM | ||
Hello! In what units is the current expressed in ST Motor pilot? And how to convert this current u...
| 2022-08-19 12:59 AM |