Subject | Author | Posted | |
---|---|---|---|
Hi, I am trying to run a brushless motor at constant speed and at a ramped input (from 0 rpm to ...
| 2022-09-22 1:24 AM | ||
Hello, I am working on a project that requires control the motor speed by adjusting bus voltage. Th...
| 2022-09-20 8:27 PM | ||
Trying to use B-G431B-ESC1 - Discovery kit with specific motors, Rs = 0.1 om, Ls =0.01 mH. STM Moto...
| 2022-09-19 2:19 PM | ||
I've got an X-NUCLEO-IHM03A1 (the PowerSTEP based board) and a NUCLEO-G431RB. I'd like to start on ...
| 2022-09-10 7:42 PM | ||
We are using STM32F301 micro along with 5.4.4 motor control SDK. We found that at different speeds ...
| 2022-09-05 1:38 AM | ||
Hello! In what units is the current expressed in ST Motor pilot? And how to convert this current u...
| 2022-08-19 12:59 AM | ||
I have a steval-dpsllck1 board. If I want to initialize due to a program problem in the board, if ...
| 2022-08-18 2:03 AM | ||
We are working on a project to control a PMSM servo motor with Encoder and Hall sensors. We have cu...
| 2022-08-15 2:55 AM | ||
Info : accepting 'gdb' connection on tcp/3333 Warn : GDB connection 2 on target STM32F031C6Tx.cpu ...
| 2022-08-08 1:40 AM | ||
Hello Can you point me to some documentation regarding the tuning of the PI control loops in moto...
| 2022-07-26 1:04 PM | ||
hello everyone, ı am trying BLDC motor driver with stm32f302R8 but ı having a problem with comp4...
| 2022-07-24 11:01 PM | ||
2022-07-12 9:17 PM | |||
2022-07-04 11:53 PM | |||
After getting the example ACIM program running (Nucleo-G431RB and STEVAL-IHM023V3), I want to custo...
| 2022-06-28 7:50 AM | ||
2022-06-27 11:05 AM | |||
Unfortunately, I cannot get MCSDK to generate the Middleware with the Induction option, as it eithe...
| 2022-06-27 6:39 AM | ||
After rigorously following the instructions numerous times with every possible STM32CubeMX, Toolcha...
| 2022-06-24 7:56 AM | ||
I'm able to develop the project for a general brushles motor but I'm not able to convert it into an...
| 2022-06-21 2:51 AM | ||
If I measure the DC supply voltage for my X-NUCLEO-IHM08M driver board - connected to a Teknic mo...
| 2022-06-07 4:48 AM | ||
The code in mc_tasks.c in routine void TSK_MediumFrequencyTaskM1(void) calls bool IsSpeedReliable ...
| 2022-06-06 9:32 AM |