User Activity

Hello Sir/Madam,I'm developing FOC motor control algorithm for our motor application. I've coded mathematical equations, PI controller and SVM. I've only current loop so I am controling torque. When I run my code, I expect that my motor will run at m...
Hi there,I'am using STEVAL-SPIN3201 evaluation board. I've reset PA11 for overcurrent output signal visible only to MCU and set PF6 and PF7 for overcurrent protection limit. Also, I've configured TIM1 channel 1 PA8 pin to center aligned pwm mode. Whe...
Hi There,I am currently working on ADC and Timer. I have 3 channels of ADC and using DMA. I want to trigger ADC at Timer1's update event. Also, I've set Timer's parameters to center aligned pwm, repetition counter to 1(with this I will trigger ADC at...
Hello there,I have sensorless 3-phase bldc motor. I am using MC Workbench for Sensorless FOC algorithm with STEVAL-SPIN3201 board. I've run my motor at torque mode and it seems okay. But, when I loaded motor does not produce any torque and immediatel...
Hello There,I am currently work on 6 - Step (Trapezoidal) Control and have developed my software with Nucleo - F302R8. I have a low inductance(23uH) bldc motor. When I've tested this motor with my software, current signal doesn't look right. Also, we...
Kudos from