Subject | Author | Posted | |
---|---|---|---|
I am integrating a TSC2007 touch controller on a Nucleo H7A3 board. I have created a simple test s...
| 2022-04-22 06:42 PM | ||
Hi, I've started a project STM32CubeMX and CubeIDE. I initialized a 4.3" TFT with LTDC and TouchGFX...
| 2022-04-19 10:54 AM | ||
Hi I'm trying to get a LCD Display run with a Nucleo U575 Board via FMC connection. I followed t...
| 2022-04-19 01:44 AM | ||
Hi TouchGFX Engineers, I have been debugging an issue while developing secure updates for a touc...
| 2022-04-18 04:58 PM | ||
On the 21st of March the new version was released. Here's the changelog: Version 4.19.0 Re...
| 2022-04-07 05:10 AM | ||
Hi, I just upgraded my touchgfx from version 16 to version 19 and I can't manage to make the proje...
| 2022-04-07 02:54 AM | ||
Display is glitches for a short moment every 20ish seconds if ICache enabled and optimization for d...
| 2022-04-06 11:00 PM | ||
I've been trying to update touchgfx display from values obtained from canbus. I dont know what the ...
| 2022-04-05 09:01 AM | ||
When I malloc the fontdata[2048] in internal RAM, it work well. But when I malloc fontdata[2048] in...
| 2022-04-05 02:28 AM | ||
It works if I write " " int the xml file or if I copy a newline from the clipboard. Holding AL...
| 2022-03-28 01:51 AM | ||
Hi, I was wondering if there is an example of using the B-CAMS-OMV with STM32F75-DK, I really tried...
| 2022-03-25 11:28 PM | ||
Code works fine in simulator but compilation to target (STM32756G-eval2). Code: // MainDisplay...
| 2022-03-24 02:04 PM | ||
2022-03-23 11:45 PM | |||
I know there is no demo that runs on a 411. I'd also have to write my own display driver to transfe...
| 2022-03-23 04:55 PM | ||
Created a simple .ioc based on STM32H733 (the same happens with STM32F429) with software packs SEGG...
| 2022-03-17 03:07 AM | ||
Hi, I've encountered a strange problem. I have two High Priority tasks and the touchGFX task se...
| 2022-03-14 11:34 PM | ||
Hi ST Employees, When I build apps using cube I have the option of generating pairs of periphera...
| 2022-03-05 04:21 PM | ||
2022-03-01 10:56 PM | |||
Hello. I was wondering if someone tried to do this or if someone has an example of how to do this. ...
| 2022-02-15 01:59 PM | ||
Hi, Seemingly the following TextArea.. widget method misreports when used with 270 degree (and p...
| 2022-02-14 03:46 AM |