Subject | Author | Posted | |
---|---|---|---|
2022-09-15 10:51 PM | |||
With the fonts placed in the external flash I got the hard fault "unaligned access". If the fonts a...
| 2022-09-15 05:16 AM | ||
Hi, I think ther is a bug on touchGFX 4.20.0 If you choose the object "static graph" Insert ...
| 2022-09-12 12:56 AM | ||
Hello, I am getting this compilation error when running simulator: error: 'mutex' in namespace '...
| 2022-09-07 02:15 AM | ||
I posted before with a question about getting the LCD to work on F746. I have that working but now ...
| 2022-08-25 09:41 AM | ||
I have a working prototype using custom board with an STM32H7 controlling, among other things, a 7"...
| 2022-08-19 07:12 AM | ||
When debugging the following part of the code I expect the program execution to stop when entering ...
| 2022-08-19 06:34 AM | ||
Hi, Sorry for the long post, I was looking at the TouchGFX documentation for UI development and...
| 2022-08-10 07:21 PM | ||
Hi all! I need to transmit data captured from DCMI to USB as a UVC Device Class. Is there any ex...
| 2022-08-10 12:44 AM | ||
Hello, in the past two days I've been trying to get working STM32L053R8T6 on my board. I managed to...
| 2022-08-05 09:09 AM | ||
Have anyone succeeded in using compressed images with TouchGFX ? Here is what I tried to do (spoile...
| 2022-07-20 07:54 AM | ||
Hi Community, Instead of BSP FT6x06 Touch Sensor (Which is connected to I2C4) how to connect to...
| 2022-07-15 05:26 AM | ||
Hi Community, I have connected SPI Display-ILI9341 to STM32F769NI board and succeeded in the dis...
| 2022-06-26 10:36 PM | ||
Hi, I am working on a project, where I need to interface STM Nucleo board with Pixy Camera. I ha...
| 2022-06-26 12:19 AM | ||
Hello I am using STM32F746 Discovery board and trying to develop customized UI by using the STM32Cu...
| 2022-06-21 11:49 PM | ||
I mean once i connect the LCD to fmc gpios (without programming it just connecting it) i get 0 as t...
| 2022-05-20 01:36 AM | ||
Currently, I am following a video to operate LCD in stm32l476 discovery board. So, I downloaded thi...
| 2022-05-15 08:36 AM | ||
Hi Everybody, I got a mikromedia Plus for STM32 board from my friend. Board schematics: https:/...
| 2022-05-10 05:30 PM | ||
I have an LCD screen (ortustech COM20H2P74ULX) connected via FMC to the STM32L4 MCU and I have some...
| 2022-05-10 01:40 AM | ||
Is there any problem with LCD driving with HYPER RAM(OCTASPI) + FLASH(QUADSPI) setting?
| 2022-04-24 11:46 PM |