LBarn.2
Associate II
since
2021-03-29
2024-04-04
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About LBarn.2
Options
Report User
User Activity
Posts
Replies
Has anyone tried to migrate from an Amulet gui (GemStudio) program to touchgfx
2022-11-03
i have been using the STM32cubeide for years. I have it loaded on 2 laptops. On one I must have made a mistake initially in the setup. It will no longer update to the next release.
2022-06-17
The computer has two Solid state drives, C is only 120 Gbytes, D is 1000 Gbytes. Currently the C drive has all the files and programs and is running out of room. What should I do? How can I use the D drive?
I am converting a project built on an STM32F072 to an STM32L071. I use a small area of flash memory to store some tables, etc. < 100 bytes. The program using the STM32IDE works fine for the F072, but I get a Hard fault with the L071.
2021-03-29
I am using page erase and HAL flash program functions
Re: I am converting a project built on an STM32F072 to an STM32L071. I use a small area of flash memory to store some tables, etc. < 100 bytes. The program using the STM32IDE works fine for the F072, but I get a Hard fault with the L071.
2021-03-30
Thanks to MM..1, I used Data eeprom and it worked perfectly, Thanks!