Subject | Author | Posted | |
---|---|---|---|
Long story short, I have a circular MIPI-DSI display and need to rotate the image by 180 deg. I've ...
| 2021-06-23 01:48 PM | ||
As I add more widgets into a screen, and each with non trivial behavior,one problem that I start to...
| 2021-06-21 05:24 AM | ||
I have STM32F407 Boards like, DIsco board (without TFT) and some basic Chinese Boards. I have inter...
| 2021-06-20 09:17 AM | ||
I am trying to get the Camera module (MB1379) running on the STM3220G-EVAL. The MB1379 has the OV56...
| 2021-06-15 08:15 AM | ||
Hello, if I try to run the simulator from inside TouchGFX 4.16.1, I get the following error. cann...
| 2021-06-14 07:06 AM | ||
Hello, I am currently trying to play a video using the JPEG decoder on a STM32F76xx chip. Rig...
| 2021-06-11 02:04 AM | ||
Hi, I am working on the ili9488 spi based display screen with touch using stm32l4r5zi nucleo kit...
| 2021-06-08 10:47 AM | ||
Hi, I am using TouchGFX into a custom board with STM32L476 and simple display with RA6963 driver. ...
| 2021-06-08 06:24 AM | ||
I have seen this thread https://community.st.com/s/question/0D53W000007XLbHSAW/why-does-animating-a...
| 2021-06-06 11:29 PM | ||
Dear Engineers, I wonder if there is any example code available with Touchgfx on how to 1) Catch...
| 2021-06-05 11:04 PM | ||
2021-06-05 07:50 AM | |||
Hi, I noticed that there is a touchgfx::memset implemented in Utils.hpp. Any reason to use touchg...
| 2021-06-04 11:18 AM | ||
Hi Use the buttons to set the sec and min. Use the START button to switch to ScreenCurrent. ...
| 2021-06-04 04:21 AM | ||
Hi everyone, I have some datas that I'd like to display inside a table on my screen without creati...
| 2021-06-04 02:38 AM | ||
As we know STM32CubeMX generates MSVC project file .sln for simulation project. I find this is real...
| 2021-06-01 08:23 PM | ||
So as I notice though the default TouchGFX RTOS is FreeRTOS but its usage is wrapper by CMSIS OS la...
| 2021-06-01 08:14 PM | ||
2021-05-29 01:58 AM | |||
MyApplication.zip is created, but .json file is not created. i do not know why? Thanks
| 2021-05-28 07:14 AM | ||
Hello everyone, I am using STM32F746G-DISC board with STM32F4DIS-CAM module which comes with OV9655...
| 2021-05-28 02:09 AM | ||
The flash loader has been successfully made. The OSPI memory mapping mode has been verified succe...
| 2021-05-27 06:56 PM |