Subject | Author | Posted | |
---|---|---|---|
For the RGB565 Framebuffer Pixel Format, the touchgfx can select external data reader。but for ...
| 2021-05-17 11:48 PM | ||
So I noticed the are two generated classes under user code section *gui folder), they are FrontendA...
| 2021-05-17 01:29 AM | ||
I add a user Widget on my screen,but when i set the modalWindow to visible there is something wrong...
| 2021-05-13 11:22 PM | ||
Due to lots of image files for UI, I need to spend around 3~4 minutes programming the external flas...
| 2021-05-13 01:25 AM | ||
Hey There, I am working on a project that will involve using a STM32H743VIT6. Its quite a comple...
| 2021-05-12 01:53 AM | ||
After a month of headbanging I have finally produced picture on the STM32F469I-DISCO with DSI 800x4...
| 2021-05-11 03:42 AM | ||
Hi Guys, Iam currently developing a GUI application using the Simulator most of the time. Now ...
| 2021-05-10 04:24 AM | ||
So I've been facing a strange error where rendering pixels within my internal RAM works without iss...
| 2021-05-06 02:42 PM | ||
Hi, I has some questions about how to save data in QSPIFLASH. I notice that when touchGFX is runni...
| 2021-05-06 12:12 AM | ||
I have been working for about 4 weeks on a project which has the STM32L4R5AIIx processor and is us...
| 2021-05-02 10:06 AM | ||
Hello, I am trying to implement bmp to jpeg encode application. I have used official STM code examp...
| 2021-05-02 04:27 AM | ||
Hello, I am new to the discovery line up. I am looking for a ST32H board with fast direct MCU c...
| 2021-04-29 09:04 AM | ||
Hello, We are struggling to implement the 1k boundary when reading/writing to a frame buffer i.e...
| 2021-04-28 04:58 AM | ||
Hello, We need to add "placeholder" data points. Such that we can have a line in the Graph (for ...
| 2021-04-28 04:40 AM | ||
2021-04-27 03:30 PM | |||
So I bought STM32769 Discovery Kit and choose the TouchGFX Designer template accordingly and the de...
| 2021-04-26 02:17 AM | ||
I feel doing a project with RTOS in TouchGFX is more complex as i don't have a knowledge in RTOS.Th...
| 2021-04-25 09:24 PM | ||
Hello there, I'm currently workimg on a TouchGFX project and I would like see how it looks simulat...
| 2021-04-22 04:05 AM | ||
Hi Guys, I am working on one of the project, in that I have to read the TouchGFX assets from Ext...
| 2021-04-20 10:22 PM | ||
When using scroll wheel with text area, the controller falls into a hard fault, when I use the func...
| 2021-04-16 09:24 PM |