User Activity

Hi All,I am developing the standby mode to achieve low power consumption due to the battery-operated device application.I have tested it with the eval kit and configured the wake source pin as well with the available user button(in blue color) connec...
Hello All,I am working on the STM32 project and using the makfile to compile and generate respective hex and bin files.I have configured all the setups using adding path in windows10 os environment variables for makefile and gnu gcc compiler.It compi...
Hi All,I am working on my Nucleo-L4R5ZI board and facing issues with firmware sdk packages downloaded by "Stm32cubeMx" and "Stm32CubeIDE" software respectively.I am just trying to test the board using simple led toggle program but it unable to make i...
Hi, Can we use ST25RU3993 Eval kit in Device mode directly(instead of Host driven), without using the GUI application.Need to use it directly without using GUI Application for making configuration for detecting the TAGs. Please let me know if such se...
Hi,I working Stm32f767zi mcu with HMI screen and I need to make communication using RJ45 interface using tcp ip. I need to know that which example is works for it, I have searched and checked a tcp ip server example code to get new incoming hmi conne...