Subject | Author | Posted | |
---|---|---|---|
According to the documentation, widgets are only redrawn once in the 'render' phase: https://suppo...
| 2021-11-04 08:08 AM | ||
Hi, The same size images, one uses format L8_RGB565 with background colour and the other uses ...
| 2021-11-03 05:26 PM | ||
Hi guys, I'm trying to make a Text Area work like a button by adding a ClickListener Mixin to it. ...
| 2021-11-03 03:38 PM | ||
Hi, I use 'makeTransition' function to animate the screen transition and the new screen has a ...
| 2021-11-02 06:09 PM | ||
Hey guys, So, I'm taking on a project that will use STM32H7 chip with a TFT panel screen (with t...
| 2021-11-02 03:25 PM | ||
Hi, I have successfully implemented a complete graphic to display some system related parameter...
| 2021-11-01 11:41 PM | ||
My DCMI setting is as follow: hdcmi.Instance = DCMI;
hdcmi.Init.SynchroMode = DCMI_SYNCHRO_HARD...
| 2021-11-01 05:39 AM | ||
Hello everyone! I'm working on a TouchGFX project on STM32F429 discovery board, because of the s...
| 2021-11-01 02:40 AM | ||
Hello, I'm working on a STM32F769I-Eval Board, and generated a TouchGFX project for it. My projec...
| 2021-10-28 08:15 AM | ||
I have custom board with 800x480 TFT display, external SDRAM and STM32H745II MCU. I have two probl...
| 2021-10-27 06:04 AM | ||
Hi, I'm trying to reduce the frame buffer size for LTDC, Therefore I'm using CLUT I configured ...
| 2021-10-25 07:34 PM | ||
Have ListLayout to which MenuItemToggle items have been "add". I believe ListLayout can be travers...
| 2021-10-24 01:27 PM | ||
Hi, I want to use a TextLabel container found in another project. I manually edited the Designer'...
| 2021-10-20 06:20 AM | ||
2021-10-18 04:02 AM | |||
Run Target Generate Done Generate Assets make -f simulator/gcc/Makefile ass...
| 2021-10-13 04:26 AM | ||
Hi, I have a custom designed board with stm32f429iit6, external SDRAM (IS45S16400J) and external N...
| 2021-10-13 01:00 AM | ||
Run Simulator Generate Done Generate Assets make -f simulator/gcc/Makefile ...
| 2021-10-12 02:33 AM | ||
I can not find a project and being new to TouchGFX, a working project is best to learn from. I can...
| 2021-10-06 01:22 PM | ||
I have a weird issue with ScrollWheel. All the elements are displayed properly. However, it seems t...
| 2021-10-04 08:46 AM | ||
According to this documentation, lockDMAToFrontPorch has a sense only for double buffer. But in fac...
| 2021-10-03 03:33 AM |