Subject | Author | Posted | |
---|---|---|---|
Dear specialist, I have to apply spi-lcd(with st7789v driver ic, 320x170) on our own ckt using stm...
| 2021-09-27 07:20 AM | ||
Due to mechanical restrictions I'm being asked to implement an Uctronics U6111 display board with S...
| 2021-09-23 08:58 AM | ||
The reason is we have noticed both the display and touchscreen freeze after 3 months in our test su...
| 2021-09-23 03:33 AM | ||
Greetings People. I am trying to interface grphics lcd ST7920 with STM32L using u8g2 and spi int...
| 2021-09-22 11:02 PM | ||
When selecting the STM32F429I-DISC1 Board, STM32CubeMX (v6.3.0) sets the LCD clock to 25MHz which i...
| 2021-09-22 01:01 AM | ||
Hi Everyone, In STM32Cube_FW_F7_V1.16.0 folder --> Utilities folder -->TouchGFX_STM32F769 some exa...
| 2021-09-16 03:19 AM | ||
2021-09-16 02:01 AM | |||
I am trying to build a smart home interface using touch gfx. After some smooth jurney, i am stuck ...
| 2021-09-15 03:08 AM | ||
I have a project that requires advanced text placement that comes from the backend. In other word...
| 2021-09-08 08:41 AM | ||
Please help me out with any algorithm to access (3000+) PGNs. So that i can access any of them from...
| 2021-09-06 06:39 AM | ||
I have a ScrollList at the end of a ScrollableContainer. If I scroll down the ScrollableContainer t...
| 2021-09-01 08:14 AM | ||
I am trying to build a smart switch using the stm32f7508 disco kit. To improve the scrolling perfo...
| 2021-09-01 06:12 AM | ||
Hello, is there an example for the cacheable containers or generally more information than in th...
| 2021-09-01 12:02 AM | ||
Hi all, I want to interface TFT LCD through RGB666 interface with STM32F429 microcontroller. LCD ...
| 2021-08-31 10:11 AM | ||
Hi All, I'm developping an custom board with an SPI Display (480x320 poixels). When I enable the ...
| 2021-08-29 11:05 AM | ||
I am communicating via SPI to the onboard gyroscope, collecting data and then printing it out to th...
| 2021-08-28 02:57 PM | ||
Hi folks. Have broken with a hit the capacitive touch screen that covers the display. A big line h...
| 2021-08-26 01:19 PM | ||
I am trying to run QSPI_Perfs example from cube pack for my stm32f746g-disc board. But the images a...
| 2021-08-23 08:39 PM | ||
Hello, This is a follow-up to my earlier question, to make a 7.2Msps digital oscilloscope using ...
| 2021-08-19 11:55 AM | ||
I would like to create android look alike GUI, wherein the top shutter to create menu items. curren...
| 2021-08-14 06:33 AM |