Subject | Author | Posted | |
---|---|---|---|
In my configuration, the tick source for touchGFX is the LTDC vsync interrupt. This was the recomme...
| 2021-12-06 12:13 PM | ||
Hello there. On my board I've setup DCMI to read some arbitrary data from ADC. I've planed to use ...
| 2021-12-04 03:51 AM | ||
Please check attached log file.
| 2021-12-03 03:57 PM | ||
I have a screen where I want to repeat a sequence of widget moves once a button is pressed, and the...
| 2021-12-02 12:18 PM | ||
Hello, I used a 32MB SDRAM and a 1GB NAND flash, the size of LCD is 480 * 800, the images save a...
| 2021-11-30 12:51 AM | ||
The specific errors are as follows
| 2021-11-24 06:46 AM | ||
Hello, I'm developing a custom board with TSC2004 touch controller, in wich i'm able to get touch ...
| 2021-11-24 02:37 AM | ||
I've been working with the L496 application template v3.0.5. In it, the touchscreen i2c memory read...
| 2021-11-23 09:10 AM | ||
I have implemented a screen transition from screen1 to screen2 upon receiving event from Backend in...
| 2021-11-15 09:01 PM | ||
I have generated the Touch GFX code by selecting STM32F769NI Discovery kit. But there is no option ...
| 2021-11-15 04:09 AM | ||
I created a project in STM32cubeIde to which I connected a graphic but when I generate in code in T...
| 2021-11-12 01:42 AM | ||
I have a project created with STM32CubeIde 1.7.1 in which through the configuration of the.ioc file...
| 2021-11-12 12:49 AM | ||
hello. touchGFX in the project I set is not going to tick. it is going to : touchgfx::HAL::taskEn...
| 2021-11-11 08:51 AM | ||
2021-11-10 10:20 AM | |||
If text is autosized, undoing will cause problems. My 4.17 Designer just froze because of it. Based...
| 2021-11-09 11:42 PM | ||
I have a TouchGFX project (using V4.17) running on IAR Workbench (V8.42.4), which consists of some ...
| 2021-11-09 10:27 AM | ||
Hi, I use flash memory ( at25sf128) in my project and I can read data from flash correctly, I chec...
| 2021-11-08 11:58 PM | ||
I want to draw a graph, and what I expect is that the data points on the left are dense and the dat...
| 2021-11-08 07:11 PM | ||
I have a GUI project with a screen size of 1024*600. There are multiple page switching in the 800*4...
| 2021-11-04 08:19 PM | ||
What could be the reason and how do I come around this problem?
| 2021-11-04 08:57 AM |