STM32 MPUs Other tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to generate elf file for Cortex M4 using IAR

Hello , This question belongs more to IAR community but still asking it .I was checking this project of OpenAMP : STM32Cube\Repository\STM32Cube_FW_MP1_V1.6.0\Projects\STM32MP157C-DK2\Applications\OpenAMP\OpenAMP_TTY_echo\STM32CubeIDE\CM4\DebugIt has...

PVaaz.1 by Associate III
  • 1895 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeMX generated build for IAR does not work

Hi   When generating for CubeIDE firmware executes fine in both production and engineering mode. But for IAR/EWARM only engineering mode works. And, yes, I am aware of production mode not supported out of the box. Manual copy to target and start requ...

PeterL by Associate III
  • 947 Views
  • 2 replies
  • 0 kudos

STM32Cube MP1 package installation on windows 10

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Install_STM32Cube_MP1_package There are only a linux path suggested, no windows path. If windows is not supported, then it is not s...

PeterL by Associate III
  • 358 Views
  • 2 replies
  • 0 kudos

Resolved! IAR and Engineering Mode

I have a STM32MP157c-DK2, programming on Windows-10.What works: Build Yocto, adapt it, flash the image to the SD-Card.Use STM32CubeIDE to program and debug code on CM4My goal is to setup a proper workflow of the project, where I can integrate our sta...

Led by Senior
  • 1707 Views
  • 20 replies
  • 0 kudos