cancel
Showing results for 
Search instead for 
Did you mean: 

What invalid HTML?

waclawekjan_0-1687588636615.png

1. I know that html is the underlying format to the posts, but other users may not be aware of it, so the formulation is confusing for them.

2. more importantly; what invalid HTML was found? I did not use the HTML edit mode in that post. I might've typed in something which offended the checker, but it should've pointed out exactly what, and not just removed something without my knowledge and consent.

How hard it may be to understand that POSTS ARE NOT TO BE MUTILATED!!! (even if it may sound as innocent as removing noses from hand-written smileys).

JW

4 REPLIES 4
Lina_DABASINSKAITE
Community manager
Community manager

Hello @waclawek.jan , 

Doublechecking on this one. Have you tried to copy/paste HTML into the post or the underlined content is typed by you? 

BR,
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Andrew Neil
Evangelist III
Andrew Neil
Evangelist III

Here's a specific example that causes the "Invalid HTML" message:

https://community.st.com/t5/feedback-forum/quot-invalid-html-quot-but-accepted-in-editor/td-p/723081

TL;DR: the HTML is not (necessarily) invalid; it may be unsupported - but it's not invalid.

Andrew Neil
Evangelist III

@waclawek.jan wrote:

1. I know that html is the underlying format to the posts, but other users may not be aware of it, so the formulation is confusing for them.


Indeed - for example:

https://community.st.com/t5/feedback-forum/quot-invalid-html-quot-errors-on-posting-a-message/m-p/607183/highlight/true#M696:~:text=There%20is%20no%20HTML%20in%20the%20message