Skip to main content
Andrew Neil
Super User
January 24, 2024
Question

Klunky Quoting

  • January 24, 2024
  • 11 replies
  • 15588 views

First, it is nice that the forum does now have some quoting ability at all; that's an improvement - thanks!

But it is rather klunky:

1. It only ever quotes an entire post in full - this is usually not helpful/useful.

A decent quoting feature would allow a part of a post to be selected and quoted.

2. Once you're inside the quote block, it seems impossible to get out of it. 
The 'Clear formatting' button doesn't work.

    This topic has been closed for replies.

    11 replies

    Peter BENSCH
    ST Technical Moderator
    January 24, 2024

    @Andrew Neil wrote:

    First, it is [...] improvement - thanks!

    (This is manually inserted within the quote)

    1. It only ever quotes an entire post in full - this[...]


    Somehow I don't understand your problem: I can insert quotes, which initially always takes the whole post. Then I can select any part of the quote block with the mouse and delete it with one keystroke, or insert my own text (e.g. here [...]). I can access the edit mode outside the quote block by clicking outside or moving using cursor keys and writing - just as I am doing now.

    Can you please explain it a bit more?

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Andrew Neil
    Super User
    January 24, 2024

    @Peter BENSCH wrote:

    I can insert quotes, which initially always takes the whole post. Then I can select any part of the quote block Can you please explain it a bit more?

    That's the first problem: you can only insert the entire post - it should be possible to select the part of the previous post that you want to cite, and have only that part inserted as a quote in the reply.

    As it stands, editing-out the excess is not so simple when the quote is long and/or contains code blocks and/or contains pictures - the selection is apt to go haywire.

    Indeed, the "getting stuck in the quote block" is hard to explain. Try this:

    1. Hit 'Reply'
    2. Hit the 'Quote' button
    3. Now you realise you want to add a comment before the quote 
    4. you can't - it's impossible to get your cursor to move before the quote block.

    Also this:

    1. Hit 'Reply'
    2. Hit the 'Quote' button
    3. Put your cursor somewhere within the quote
    4. Hit Ctrl+Shift+End to select all of the rest of the quote
    5. Delete the selected text
    6. You are now stuck in the quote block - you can't move the cursor beyond it, and hitting Return will just extend the quote.
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Peter BENSCH
    ST Technical Moderator
    January 24, 2024

    Ah, interesting... I can confirm it, but I hadn't tried it yet.

    @Laurids_PETERSEN @Lina_DABASINSKAITE 

     

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Andrew Neil
    Super User
    January 24, 2024

    There's another annoying limitation:

    You can only quote from the one post you're replying to - you can't bring in quotes from other posts.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    waclawek.jan
    Super User
    January 24, 2024

    This is Khoros, a customer experience engagement platform (mixing/matching some of the buzzwords from their web, I'm really not interested in how exactly they call it). NOT a forum software, so don't expect rudimentary forum features crystalized throughout the three or four decades of technical fora. It's an ajaxoid primarily aimed at a simplistic one or two exchange of a sales person with a customer, designed to "impress", not to be usable. With emphasis on such important features as emoticons.

    In HTML view, you can use the "blockquote" tag, if you want, and it surprisingly does what you expect; but I mostly just go for a simple manually inserted ">" (hardly something which would go well with "engagement"). Yeah, can't insert sane manual line break so only one ">" at the beginning of the quote.

    JW

    Laurids_PETERSEN
    ST Community Manager
    February 14, 2024

    Hello everyone,

    Adjusting the quote function requires more extensive customization than initially estimated. It's on the list of improvements for the community moving forward. 

    As always, thanks for providing your feedback. Your opinions and insights are appreciated. 

    Best regards,
    Laurids  

    Andrew Neil
    Super User
    December 20, 2024

    Still an ongoing annoyance - and it seems I'm not the only one annoyed by it:

    https://community.st.com/t5/feedback-forum/how-to-properly-use-the-quote-tool/td-p/755735

    @eduardo_reis 

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.