2024-03-18 8:32 AM
Here, in the thread "Over Current on STM32 Board", the same thread is listed as 'Related Content' !
:face_with_tears_of_joy:
It's not "Related" content - it's exactly the same content!
I think this happened because I came to a specific post within that thread (from a Notification) - rather than a link to the top of the thread?
2024-03-19 6:48 AM
Hello @Andrew Neil ,
Thanks for bringing this to our attention. We will further investigate to understand the reported behavior and get back to you as soon as we have some updates.
If there is anything else in the meantime, just let us know.
Best,
Amelie
2024-03-19 6:53 AM
it just happened again:
This was definitely coming from the link in a notification email to a reply post later in the thread.
Note the "RE:" in the heading right at the top...
2024-03-19 7:45 AM
and another - this time via the "bell" icon in the forum:
2024-03-25 6:59 AM
A simple, effective solution which won't harm anything is to remove "Related Content" entirely... :)
JW
2024-07-01 6:15 AM
Hello @Andrew Neil , all,
This issue has been sorted. Let us know if it works on your end too.
Lina
2024-07-01 7:40 AM
Yes, it does now seem to be fixed!
:thumbs_up: :beaming_face_with_smiling_eyes:
2024-07-01 7:56 AM
Not sure I agree there, it's honestly more on point than the usual search methods half the time.
What I'd like to see is more of this BEFORE people post basically the same question OVER AGAIN for the N-th time..
The circular thing Andrew points out is a bit daft, seen that a few time, if that's fixed great, swear I saw it this morning, but will be watching now.
2024-07-02 4:01 AM
2024-07-02 4:32 AM
Thanks for informing! I will have it checked.