cancel
Showing results for 
Search instead for 
Did you mean: 

Zoom control for ALL attached images request

MM..1
Chief III

Example image without zoom controll

Re: ThreadX thread and queue names not displayed p... - STMicroelectronics Community

example with zoom controll i cant found now , but sometimes is showed bottom on image 

MM1_0-1717516867907.png

 

and i mean this zoom control is required on all any image. 

5 REPLIES 5
Lina_DABASINSKAITE
Community manager

Hello @MM..1 , 

Thanks for sharing your request. I will see what we can do about it and get back. 

In the meantime, I suggest using a workaround following these steps: 
1. Right mouse click on the image
2. Select "Magnify image" 

This will allow you to have a zoom in / zoom out option. 

Cheers,
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Definitely see inconsistency, perhaps related to the image type. ie for PNG but not JPG ?

Also find the two-point finger stretching on Android is frustrating, and also having to down load attached images to see them.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi @MM..1 @Tesla DeLorean ,

Could you please share a direct link when you come across an image with the zoom control you are referring to? We need an example to be able to investigate it.

Best,

Adam

Error in final launch sequence - STMicroelectronics Community attached png show zoom

normal images no. But on my notebook with 2560x1440 14inch is ...

Hi @MM..1 ,

Zoom controller is currently only available for file attachment previews. We will pass along the topic to the developer team to understand the effort involved in adding a zoom controller for images in posts. Depending on the estimation, we will decide how to move forward with this topic. We will keep you posted.

Best,

Adam