cancel
Showing results for 
Search instead for 
Did you mean: 

Distinguish "information" posts from questions

Andrew Neil
Evangelist III

There's a lot of "information" posts appearing; eg,

AndrewNeil_0-1706630711548.png

https://community.st.com/t5/stm32-mcus/how-to-obtain-and-use-the-stm32-96-bit-uid/ta-p/621443

This is all very good & useful but, in the activity listing, they are indistinguishable from user questions:

AndrewNeil_1-1706630853302.png

It would be useful if these were clearly differentiated.

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Andrew Neil 

We released an update today that marks articles on the front page activity feed with a little "book" logo. 
When hovering over the logo, it states "Knowledge base article." 

This should help distinguish articles from posts, see example below:

Laurids_PETERSEN_1-1709030341470.png

Best regards,
Laurids

View solution in original post

9 REPLIES 9
Lina_DABASINSKAITE
Community manager
Community manager

Hello @Andrew Neil , 

Thanks for your feedback here. It is a very good point indeed. I will take it to discuss internally how we could distinguish Knowledgebase articles from regular posts. 

If you have any preferences, please share! 

BR,
Lina


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Don't you already have a tag or sub-forum specifically for Knowledge Base articles?

When logged in, what's displayed should track what you're subscribed too / following.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi @Tesla DeLorean , 

Yes, there is a separate section for it, but on the general activity feed, you can not tell weather a post is a questions or an article. 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Andrew Neil
Evangelist III

Another couple today:

AndrewNeil_0-1708353671334.png

Really hard to tell that "How to add your spi flash into the STM32CubeProgrammer's External Loader" isn't a question.

@B.Montanari 

Hi @Andrew Neil

These titles are given to be more attractive to search engines. We are working on creating a solution that visually marks the post as an article, just like how a post with a solution has the green checkmark.

Best regards,
Laurids  


Andrew Neil
Evangelist III

@samnere no need to quote the entire post - just 'Subscribe':

AndrewNeil_0-1708361539373.png

 

Hi @Andrew Neil 

We released an update today that marks articles on the front page activity feed with a little "book" logo. 
When hovering over the logo, it states "Knowledge base article." 

This should help distinguish articles from posts, see example below:

Laurids_PETERSEN_1-1709030341470.png

Best regards,
Laurids

Thanks - I'll keep a lookout for that ...

Just seen one:

 

AndrewNeil_0-1709053462142.png

 

:thumbs_up: