2024-07-23 2:41 AM - edited 2024-07-23 3:30 AM
I am trying to get the accuracy of the model by validating of desktop. But when I provide npz files for Validation inputs and outputs it gives me an error as shown in the screenshot. When I give only one1 npz file validates successfully but cannot give accuracy because of no output data.
Solved! Go to Solution.
2024-07-23 4:09 AM
As stated in the documentation if you provide an npz with the input and the output just use the --vi option
-vi/valinput |
indicates the custom test data set which must be used. If not defined an internal self-generated random data set is used (refer to [METRIC], “Input validation files” section) - Optional |
-vo/valoutput |
indicates the expected custom output values. If the data are already provided in a simple file ('*.npz' ) through the '-vi' option this argument is skipped - Optional |
2024-07-23 4:09 AM
As stated in the documentation if you provide an npz with the input and the output just use the --vi option
-vi/valinput |
indicates the custom test data set which must be used. If not defined an internal self-generated random data set is used (refer to [METRIC], “Input validation files” section) - Optional |
-vo/valoutput |
indicates the expected custom output values. If the data are already provided in a simple file ('*.npz' ) through the '-vi' option this argument is skipped - Optional |